VIL Spec of GPIO DC Parameter for i.MX6ULL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VIL Spec of GPIO DC Parameter for i.MX6ULL

Jump to solution
1,077 Views
ko-hey
Senior Contributor II

Hi all

 

Let me ask about VIL min spec of GPIO for i.MX6ULL.

 

I'm checking a Table 24 in following document.

https://www.nxp.com/docs/en/data-sheet/IMX6ULLIEC.pdf

 

According to the table, the Min of VIL is 0 V.

217782_217782.jpgimage003.jpg

 

I think that the Min spec is stricter than general GPIO spec.

Do you have any reason that the spec is stricter than general spec ?

 

Furthermore, it was changed from 0 V to -0.3 V in the datasheet of i.MX7D.

Do you have any possibility that the spec of VIL for i.MX6ULL will be changed as same as i.MX7D ?

 

Ko-hey

 

Labels (3)
0 Kudos
Reply
1 Solution
886 Views
Yuri
NXP Employee
NXP Employee

Hello,

 There are no plans to modify the VIL parameter; instead, it had been described as Overshoot and undershoot conditions in the datasheet.

 

GPIO_overshoot_undershoot.PNG

 

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
4 Replies
886 Views
Yuri
NXP Employee
NXP Employee

Hello,

   The table "Absolute Maximum Ratings" contains the following specs:

Input/Output Voltage Range Vin/Vout  min = -0.5 V  max= OVDD+0.3 V
(OVDD is the I/O supply voltage).

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
886 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

I'm talking about operating range.

We're concerning about whether any possibility that the spec of VIL for i.MX6ULL will be changed or not as it like i.MX7D.

Please check following tables.

One is IMX7DCEC Rev.D.

image005.jpg

The other is IMX7DCEC Rev.5

image006.jpg

The operating range was changed.

I know that almost of the IP for i.MX6ULL is same as i.MX7D.

As a result, I think it will be changed the spec of VIL for i.MX6ULL if the spec of i.MX7D was changed.

Do you have any possibility that the spec of VIL for i.MX6ULL will be changed as same as i.MX7D ?

Ko-hey

0 Kudos
Reply
887 Views
Yuri
NXP Employee
NXP Employee

Hello,

 There are no plans to modify the VIL parameter; instead, it had been described as Overshoot and undershoot conditions in the datasheet.

 

GPIO_overshoot_undershoot.PNG

 

Regards,

Yuri.

0 Kudos
Reply
886 Views
ko-hey
Senior Contributor II

Hi Yuri Muhin

Thanks!!

Ko-hey

0 Kudos
Reply