Dear Sir
I want to ask about the VDD_ARM_IN and VDD_SOC_IN of i.MX6Dual.
I understand that there is the following merit when dividing the power supply of VDD_ARM_IN and VDD_SOC_IN.
It is able to reduce the power consumption by setting an appropriate voltage for each.
Q1.
Are there any problem when it is not separated the power supply for VDD_ARM_IN and VDD_SOC_IN.
Best Regards,
Eishi SHIBUSAWA
Hello,
VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source,
assuming the supply can provide proper current load / capacity.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------