VDD_xxx_IN

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

VDD_xxx_IN

393件の閲覧回数
eishishibusawa
Contributor III

Dear Sir

 

I want to ask about the VDD_ARM_IN and VDD_SOC_IN of i.MX6Dual.

I understand that there is the following merit when dividing the power supply of VDD_ARM_IN and VDD_SOC_IN.

It is able to reduce the power consumption by setting an appropriate voltage for each.

 

Q1.

Are there any problem when it is not separated the power supply for VDD_ARM_IN and VDD_SOC_IN.

 

Best Regards,

Eishi SHIBUSAWA

ラベル(1)
0 件の賞賛
返信
1 返信

299件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  VDD_ARM_IN and VDD_SOC_IN may be supplied from the same source,

assuming the supply can provide proper current load / capacity.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信