On our board we would like to use a RGMII-PHY together with i.MX6DL.
The MAC and PHY are connected similiar to the SABRE reference board, the main difference is that the ENET_REFCLK pin which is not connected at all.
I assume this is OK, according to the "Hardware Development Guide" (chapter 12.3 Generating the reference clock) "the pin labeled “ENET_REF_CLK” in Figure 12-2 is only required by the full MII interface.
It is not used by the RMII interface."
Based on this I made further customization (compared to the "sabre-sd" board configuration):
* setting bit ENET_CLK_SEL in GPR1
* configuring (internal) ENET PLL to generate ethernet reference clock (125Mhz),
Unfortunatelly u-boot fails to ping another host, I'm getting "TX timeout packet" error. I suppose this could be caused by missing reference clock.
I checked already that management interface to the PHY works but the RGMII_TXC line doesn't show any activity (during ping command).
Did anybody encounter similiar problems?
Is it possible to route ENET PLL to ENET_REF_CLK (internally - using IOMUX) or does it have to be routed externally (i.e. from GPIO16 or PHY generating 125Mhz)?
Thank you for any feedback
已解决! 转到解答。
Chapter 11 (Using the RMII Interface) of the Hardware Development Guide for
i.MX6 describes RMII options : "There are two possible pins that can either
source or sink the reference clock: GPIO_16 and RGMII_TX_CTL."
GPIO_16 is intended for RMII reference clock; ENET_REF_CLK is intended for
RGMII reference clock. Next, ENET_REF_CLK is input clock, that is - an external
source should be applied - this has been validated.
Note that the ENET_REF_CLK input on MX6 is fed via NVCC_ENET supply rail.
The internal source has to be routed externally from GPIO_16 to ENET_REF_CLK.
So even if customers use the internal clock they would still need to bring
it back in on the ENET_REF_CLK pin.
Chapter 11 (Using the RMII Interface) of the Hardware Development Guide for
i.MX6 describes RMII options : "There are two possible pins that can either
source or sink the reference clock: GPIO_16 and RGMII_TX_CTL."
GPIO_16 is intended for RMII reference clock; ENET_REF_CLK is intended for
RGMII reference clock. Next, ENET_REF_CLK is input clock, that is - an external
source should be applied - this has been validated.
Note that the ENET_REF_CLK input on MX6 is fed via NVCC_ENET supply rail.
The internal source has to be routed externally from GPIO_16 to ENET_REF_CLK.
So even if customers use the internal clock they would still need to bring
it back in on the ENET_REF_CLK pin.