Usage of Signal M4_NMI / M7_NMI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Usage of Signal M4_NMI / M7_NMI

Jump to solution
774 Views
Niebel-TQ
Contributor IV

i.MX8MQ / i.MX8MM / i.MX8MN has the opportunity tho mux this signal on PAD GPIO1_IO05. In the reference manual ist only a link to CortexM Documentation from ARM

In the implementatation of above called SOC: is this signal an input to trigger the NMI exception our an Output signalling the occurence of the exception? What is the active level of the signal - Low or High?

Thanks in Advance

Markus

 

Labels (1)
0 Kudos
Reply
1 Solution
768 Views
igorpadykov
NXP Employee
NXP Employee

Hi Markus

 

it is input to trigger the NMI exception, active level high.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
769 Views
igorpadykov
NXP Employee
NXP Employee

Hi Markus

 

it is input to trigger the NMI exception, active level high.

 

Best regards
igor

0 Kudos
Reply