Usage of SNVS_TAMPERx pin in i.MX7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Usage of SNVS_TAMPERx pin in i.MX7

跳至解决方案
979 次查看
ko-hey
Senior Contributor II

Hi all

Let me confirm about the usage of SNVS_TAMPERx pins.

Q1.

According to the table 97 and 100 in datasheet, the Power Group of those pins are VDDD_SNVS_1P8_CAP.

It should connect to VDDD_SNVS_1P8_CAP when user do external pull-up.

Am I correct ?

I'm referring the following document.

http://www.nxp.com/assets/documents/data/en/data-sheets/IMX7DCEC.pdf 

Q2.

Could you tell me the Vih and Vil value of SNVS_TAMPERx pin when user use it as a input ?

Q3.

Could you tell me the Voh and Vol value of SNVS_TAMPERx pin when user use it as a output ?

Ko-hey

标签 (3)
0 项奖励
回复
1 解答
732 次查看
art
NXP Employee
NXP Employee

A1. Yes, your understanding is correct.

A2. The TAMPER pins can be treated as regular GPIOs, so, for the 1.8V power domain, the upper Vil margin is 1.8V * 0.3 = 0.54V and the lower Vih margin is 1.8V * 0.7 = 1.26V.

A3. The TAMPER pins can be treated as regular GPIOs, so, for the 1.8V power domain, the upper Vol margin is 1.8V * 0.2 = 0.36V and the lower Voh margin is 1.8V * 0.8 = 1.44V.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
733 次查看
art
NXP Employee
NXP Employee

A1. Yes, your understanding is correct.

A2. The TAMPER pins can be treated as regular GPIOs, so, for the 1.8V power domain, the upper Vil margin is 1.8V * 0.3 = 0.54V and the lower Vih margin is 1.8V * 0.7 = 1.26V.

A3. The TAMPER pins can be treated as regular GPIOs, so, for the 1.8V power domain, the upper Vol margin is 1.8V * 0.2 = 0.36V and the lower Voh margin is 1.8V * 0.8 = 1.44V.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复