Hi all,
After android booting in UI "unfortunately the process com.android.phone has stopped" pop-up coming continuously. how to fix it.
LOGCAT:
root@sabresd_6dq:/ # logcat
--------- beginning of /dev/log/main
W/AudioService( 1029): onLoadSoundEffects() called before boot complete
I/Process ( 1277): Sending signal. PID: 1277 SIG: 9
--------- beginning of /dev/log/system
I/ActivityManager( 1029): Process com.android.phone (pid 1277) has died.
I/ActivityManager( 1029): Start proc com.android.phone for restart com.android.phone: pid=1299 uid=1001 gids={41001, 3002, 3001, 3003, 1028, 1015}
D/AndroidRuntime( 1299): Shutting down VM
W/dalvikvm( 1299): threadid=1: thread exiting with uncaught exception (group=0x2c56cba8)
E/AndroidRuntime( 1299): FATAL EXCEPTION: main
E/AndroidRuntime( 1299): Process: com.android.phone, PID: 1299
E/AndroidRuntime( 1299): java.lang.RuntimeException: Unable to create application com.android.phone.PhoneApp: java.lang.NullPointerException: missing IConnectivityManager
E/AndroidRuntime( 1299): at android.app.ActivityThread.handleBindApplication(ActivityThread.java:4331)
E/AndroidRuntime( 1299): at android.app.ActivityThread.access$1500(ActivityThread.java:135)
E/AndroidRuntime( 1299): at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1256)
E/AndroidRuntime( 1299): at android.os.Handler.dispatchMessage(Handler.java:102)
E/AndroidRuntime( 1299): at android.os.Looper.loop(Looper.java:136)
E/AndroidRuntime( 1299): at android.app.ActivityThread.main(ActivityThread.java:5001)
E/AndroidRuntime( 1299): at java.lang.reflect.Method.invokeNative(Native Method)
E/AndroidRuntime( 1299): at java.lang.reflect.Method.invoke(Method.java:515)
E/AndroidRuntime( 1299): at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:785)
E/AndroidRuntime( 1299): at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:601)
E/AndroidRuntime( 1299): at dalvik.system.NativeStart.main(Native Method)
E/AndroidRuntime( 1299): Caused by: java.lang.NullPointer
Regards,
Aravinth
you need to clear data and cache of SIM Toolkit
you can found other solutions here
The most likely cause of the issue is that the Phone application doesn't find the actual phone communication hardware present in the system. Just avoid to start the Phone application.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------