Hi NXP Team,
I am trying to flash the emmc on the imx6ull EVK board using UUU tool, but I am not able to do so. I have taken the prebuilt images from the NXP website (LF_v6.1.22-2.0.0_images_IMX6UL7D.zip). I am using Ubuntu 18.04.
The command I am using to flash is:
$ sudo ./uuu -v uuu.auto-imx6ull14x14evk
I am using the auto script provided in the above-mentioned zip package.
Here's the screenshot of the error I am getting while flashing.
Here are the console logs of the EVK.
Any suggestion to solve the issue will be very helpful!
Thanks in advance.
Regards
Meetali Patel
Hi @Gorka_3!
Are you putting the board on download mode?
Try to unzip the file and put this command:
Uuu -b emmc_all iu-boot-imx6ull14x14evk_emmc.imx imx-image-full-imx6ul7d.wic
Notes:
use sudo if you are using Linux
Run as administrator PowerShell if you are using Windows
Best Regards!
Chavira
Hi @Chavira
I have kept the board in serial download mode. I have made the switch settings for SW601 as OFF, ON, ON, OFF and SW602 as OFF, ON (referred the following screenshots from i.MX6ULL EVK Board Hardware User Guide.)
Yes, I am using the sudo command. I did try the command you gave, the same result.
Regards
Meetali Patel