Unable to flash emmc on imx6ull EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to flash emmc on imx6ull EVK

485 Views
meetalipatel
Contributor III

Hi NXP Team,

I am trying to flash the emmc on the imx6ull EVK board using UUU tool, but I am not able to do so. I have taken the prebuilt images from the NXP website (LF_v6.1.22-2.0.0_images_IMX6UL7D.zip). I am using Ubuntu 18.04.

The command I am using to flash is:

 $ sudo ./uuu -v uuu.auto-imx6ull14x14evk

I am using the auto script provided in the above-mentioned zip package. 

Here's the screenshot of the error I am getting while flashing.

meetalipatel_1-1710249976662.png

Here are the console logs of the EVK.

meetalipatel_0-1710249937356.png

Any suggestion to solve the issue will be very helpful!

Thanks in advance.

 

Regards
Meetali Patel

 

0 Kudos
Reply
5 Replies

467 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @Gorka_3!

Are you putting the board on download mode?

 

Try to unzip the file and put this command:

 

Uuu -b emmc_all iu-boot-imx6ull14x14evk_emmc.imx imx-image-full-imx6ul7d.wic

 

Notes:

use sudo if you are using Linux

Run as administrator PowerShell if you are using Windows

 

Best Regards!

Chavira

 

0 Kudos
Reply

465 Views
meetalipatel
Contributor III

Hi @Chavira 

I have kept the board in serial download mode. I have made the switch settings for SW601 as OFF, ON, ON, OFF and SW602 as OFF, ON (referred the following screenshots from i.MX6ULL EVK Board Hardware User Guide.)

meetalipatel_1-1710312576783.png

 

meetalipatel_0-1710312571619.png

 

Yes, I am using the sudo command. I did try the command you gave, the same result.

Regards
Meetali Patel

 

0 Kudos
Reply

442 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @meetalipatel!

The iMX6ull evk by default doesn't have emmc soldered.

Have you soldered the necessary components to use the emmc in imx6ull evk?

Chavira_0-1710430797015.png

 



Best Regards!
Chavira

0 Kudos
Reply

435 Views
meetalipatel
Contributor III

Hi @Chavira 

I am not aware of this. Can you please give me more details on what hardware changes needs to be done?

Thanks & Regards
Meetali Patel

0 Kudos
Reply

432 Views
Chavira
NXP TechSupport
NXP TechSupport

Hi @meetalipatel!

Check and solder the next components

Chavira_0-1710509823427.png

 

0 Kudos
Reply