Hello All ,
When I building android(Lollipop 5.0.0.1) for imx6slevk board , system.img is not able to generate.
Following error is obtained:
Install system fs image: out/target/product/evk_6sl/system_sparse.img
out/target/product/evk_6sl/system_sparse.img+out/target/product/evk_6sl/obj/PACKAGING/recovery_patch_intermediates/recovery_from_boot.p maxsize=481738752 blocksize=4224 total=403801046 reserve=4866048
if [ true = true ]; then \
simg2img out/target/product/evk_6sl/system_sparse.img out/target/product/evk_6sl/system.img; \
fi
/bin/bash: line 1: simg2img: command not found
make: *** [out/target/product/evk_6sl/system_sparse.img] Error 127
make: *** Deleting file `out/target/product/evk_6sl/system_sparse.img'
I have installed all package listed in the Android User guide as well as Establishing a Build Environment | Android Open Source Project
still any package are missing...?
please help me sort out this issue...
Regards,
Kishore P
已解决! 转到解答。
Hello Gusarambula ,
I have give the full path with the "simg2img" to solve the issue.
if [ true = true ]; then \
/home/test/Android_Source/out/host/linux-x86/bin/simg2img out/target/product/evk_6sl/system_sparse.img out/target/product/evk_6sl/system.img; \
fi
Regards,
Kishore P
Hello Kishore Poojari,
Are you still experiencing issues building Android? Have you followed the Android User’s Guide step by step? If so, did you receive any error message when downloading or patching the source code?
Hello Gusarambula ,
I have give the full path with the "simg2img" to solve the issue.
if [ true = true ]; then \
/home/test/Android_Source/out/host/linux-x86/bin/simg2img out/target/product/evk_6sl/system_sparse.img out/target/product/evk_6sl/system.img; \
fi
Regards,
Kishore P