Hi, our custom board design are following the I.MX8M PLUS EVK design(Same LPDDR4 RAM), but our custom board unable to boot up and no error message output on UART(A53). May i know how to continue to debug to narrow down the issue ? (We are suspecting the LPDDR4 RAM issue.)
已解决! 转到解答。
Hi @Jimmychea ,
Obviously, it is NOT the problem of UART but the DDR training was NOT passed compared to the log I shared. You'd better ensure that the DDR stress testing had been passed as well before generating the lpddr4_timing.c file used in u-Boot.
Best Regards,
Khang
Hi @Jimmychea ,
If you suspect the LPDDR4 issue, you can enable relevant debugging messages. Mine is for LF5.10.72:
From e79f996f4fb168a52ebc67e00c8bb05fd02d7460 Mon Sep 17 00:00:00 2001
From: l4es <linux4es@gmail.com>
Date: Fri, 21 Jul 2023 11:09:49 +0700
Subject: [PATCH 2/3] drivers: ddr: Enable debugging for DDR memory
---
drivers/ddr/imx/imx8m/Makefile | 2 ++
1 file changed, 2 insertions(+)
diff --git a/drivers/ddr/imx/imx8m/Makefile b/drivers/ddr/imx/imx8m/Makefile
index bd9bcb8d53..dd68d40544 100644
--- a/drivers/ddr/imx/imx8m/Makefile
+++ b/drivers/ddr/imx/imx8m/Makefile
@@ -4,6 +4,8 @@
# SPDX-License-Identifier: GPL-2.0+
#
+KBUILD_CFLAGS += -D DEBUG=1
+
ifdef CONFIG_SPL_BUILD
obj-$(CONFIG_IMX8M_DRAM) += helper.o ddrphy_utils.o ddrphy_train.o ddrphy_csr.o ddr_init.o
endif
--
2.17.1
And relevant messages on the console would be :
U-Boot SPL 2021.04-lf_v2021.04+g35b1ab7774 (Sep 27 2022 - 02:05:23 +0000) DDRINFO: start DRAM init DDRINFO: cfg clk DDRINFO: DRAM rate 3000MTS DDRINFO: ddrc config start DDRINFO: ddrc config done DDRINFO:ddrphy config start DRAM PHY training for 3000MTS check ddr_pmu_train_imem code check ddr_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr_pmu_train_dmem code pass [PMU Major message = 0x0000000d] [PMU Major message = 0x00000000] [PMU Major message = 0x00000002] [PMU Major message = 0x00000001] [PMU Major message = 0x0000000a] [PMU Major message = 0x000000fd] [PMU Major message = 0x000000fe] [PMU Major message = 0x00000004] [PMU Major message = 0x00000003] [PMU Major message = 0x00000009] [PMU Major message = 0x00000007] Training PASS DRAM PHY training for 400MTS check ddr_pmu_train_imem code check ddr_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr_pmu_train_dmem code pass [PMU Major message = 0x0000000d] [PMU Major message = 0x00000000] [PMU Major message = 0x00000002] [PMU Major message = 0x00000001] [PMU Major message = 0x000000fd] [PMU Major message = 0x000000fe] [PMU Major message = 0x00000004] [PMU Major message = 0x00000003] [PMU Major message = 0x00000009] [PMU Major message = 0x00000007] Training PASS DRAM PHY training for 100MTS check ddr_pmu_train_imem code check ddr_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr_pmu_train_dmem code pass [PMU Major message = 0x0000000d] [PMU Major message = 0x00000000] [PMU Major message = 0x00000002] [PMU Major message = 0x00000001] [PMU Major message = 0x000000fd] [PMU Major message = 0x000000fe] [PMU Major message = 0x00000004] [PMU Major message = 0x00000003] [PMU Major message = 0x00000009] [PMU Major message = 0x00000007] Training PASS DRAM PHY training for 3000MTS check ddr_pmu_train_imem code check ddr_pmu_train_imem code pass check ddr4_pmu_train_dmem code check ddr_pmu_train_dmem code pass [PMU Major message = 0x00000000] [PMU Major message = 0x00000006] [PMU Major message = 0x00000006] [PMU Major message = 0x00000005] [PMU Major message = 0x00000005] [PMU Major message = 0x00000007] Training PASS DDRINFO: ddrphy config done DDRINFO:ddrphy calibration done DDRINFO: ddrmix config done SEC0: RNG instantiated Normal Boot WDT: Not found! Trying to boot from BOOTROM image offset 0x8000, pagesize 0x200, ivt offset 0x0 NOTICE: BL31: v2.4(release):lf-5.10.72-2.2.3-0-g5f3ed37b8 NOTICE: BL31: Built : 09:02:12, Oct 12 2022
Hi @Jimmychea ,
Obviously, it is NOT the problem of UART but the DDR training was NOT passed compared to the log I shared. You'd better ensure that the DDR stress testing had been passed as well before generating the lpddr4_timing.c file used in u-Boot.
Best Regards,
Khang