Unable to boot up the i.MX8M Plus, even no UART message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to boot up the i.MX8M Plus, even no UART message

Jump to solution
1,521 Views
Jimmychea
Contributor III

Hi, our custom board design are following the I.MX8M PLUS EVK design(Same LPDDR4 RAM), but our custom board unable to boot up and no error message output on UART(A53). May i know how to continue to debug to narrow down the issue ? (We are suspecting the LPDDR4 RAM issue.)

Labels (1)
0 Kudos
Reply
1 Solution
1,455 Views
khang_letruong
Senior Contributor III

Hi @Jimmychea ,

Obviously, it is NOT the problem of UART but the DDR training was NOT passed compared to the log I shared. You'd better ensure that the DDR stress testing had been passed as well before generating the lpddr4_timing.c file used in u-Boot.

Best Regards,

Khang

View solution in original post

0 Kudos
Reply
7 Replies
1,512 Views
Jimmychea
Contributor III

But i can't see any output message via UART? After enable debugging message, i should see any output messages ?

0 Kudos
Reply
1,507 Views
khang_letruong
Senior Contributor III

So that might not be the issue of LPDDR4 as you said. That could be inverted Tx, Rx because the BootROM could send some message out.

0 Kudos
Reply
1,514 Views
khang_letruong
Senior Contributor III

Hi @Jimmychea ,

If you suspect the LPDDR4 issue, you can enable relevant debugging messages. Mine is for LF5.10.72: 

 

From e79f996f4fb168a52ebc67e00c8bb05fd02d7460 Mon Sep 17 00:00:00 2001
From: l4es <linux4es@gmail.com>
Date: Fri, 21 Jul 2023 11:09:49 +0700
Subject: [PATCH 2/3] drivers: ddr: Enable debugging for DDR memory

---
 drivers/ddr/imx/imx8m/Makefile | 2 ++
 1 file changed, 2 insertions(+)

diff --git a/drivers/ddr/imx/imx8m/Makefile b/drivers/ddr/imx/imx8m/Makefile
index bd9bcb8d53..dd68d40544 100644
--- a/drivers/ddr/imx/imx8m/Makefile
+++ b/drivers/ddr/imx/imx8m/Makefile
@@ -4,6 +4,8 @@
 # SPDX-License-Identifier:     GPL-2.0+
 #

+KBUILD_CFLAGS += -D DEBUG=1
+
 ifdef CONFIG_SPL_BUILD
 obj-$(CONFIG_IMX8M_DRAM) += helper.o ddrphy_utils.o ddrphy_train.o ddrphy_csr.o ddr_init.o
 endif
-- 
2.17.1

 

 

And relevant messages on the console would be :

U-Boot SPL 2021.04-lf_v2021.04+g35b1ab7774 (Sep 27 2022 - 02:05:23 +0000)
DDRINFO: start DRAM init
DDRINFO: cfg clk
DDRINFO: DRAM rate 3000MTS
DDRINFO: ddrc config start
DDRINFO: ddrc config done
DDRINFO:ddrphy config start
DRAM PHY training for 3000MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x0000000a]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 400MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 100MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x0000000d]
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000002]
[PMU Major message = 0x00000001]
[PMU Major message = 0x000000fd]
[PMU Major message = 0x000000fe]
[PMU Major message = 0x00000004]
[PMU Major message = 0x00000003]
[PMU Major message = 0x00000009]
[PMU Major message = 0x00000007]
Training PASS
DRAM PHY training for 3000MTS
check ddr_pmu_train_imem code
check ddr_pmu_train_imem code pass
check ddr4_pmu_train_dmem code
check ddr_pmu_train_dmem code pass
[PMU Major message = 0x00000000]
[PMU Major message = 0x00000006]
[PMU Major message = 0x00000006]
[PMU Major message = 0x00000005]
[PMU Major message = 0x00000005]
[PMU Major message = 0x00000007]
Training PASS
DDRINFO: ddrphy config done
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
WDT:   Not found!
Trying to boot from BOOTROM
image offset 0x8000, pagesize 0x200, ivt offset 0x0
NOTICE:  BL31: v2.4(release):lf-5.10.72-2.2.3-0-g5f3ed37b8
NOTICE:  BL31: Built : 09:02:12, Oct 12 2022
0 Kudos
Reply
1,482 Views
Jimmychea
Contributor III

Can you provide the steps on how to add the debug messages into BSP and rebuild ?

0 Kudos
Reply
1,461 Views
Jimmychea
Contributor III

I able to enable the debug messages into Uboot. The below picture showing the DDR log messages, may i know what is the issue, and how to resolve it ? Thanks

0 Kudos
Reply
1,456 Views
khang_letruong
Senior Contributor III

Hi @Jimmychea ,

Obviously, it is NOT the problem of UART but the DDR training was NOT passed compared to the log I shared. You'd better ensure that the DDR stress testing had been passed as well before generating the lpddr4_timing.c file used in u-Boot.

Best Regards,

Khang

0 Kudos
Reply
1,436 Views
Jimmychea
Contributor III

ya, UART issue and LPDDR4 RAM issue have been resolved, but i encountered new issue, i will create a new post for it. Thanks.

0 Kudos
Reply