Hello Guys,
There is an use case in which I need to flash a Linux BSP on my iMX8QXP board thorough UART port since only that port is available. How do I configure the UUU tool to flash the board using the UART port ?
解決済! 解決策の投稿を見る。
Hi @ahmedmd,
I hope you are doing well.
i.MX8QXP does not support flashing or downloading bootimage over UART.
It only supports USB 2.0 OTG and USB 3.0 ports.
Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.
Thanks & Regards,
Dhruvit Vasavada
Hi @ahmedmd,
I hope you are doing well.
i.MX8QXP does not support flashing or downloading bootimage over UART.
It only supports USB 2.0 OTG and USB 3.0 ports.
Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.
Thanks & Regards,
Dhruvit Vasavada