UUU tool using UART Port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

UUU tool using UART Port

Jump to solution
298 Views
ahmedmd
Contributor II

Hello Guys,

There is an use case in which I need to flash a Linux BSP on my iMX8QXP board thorough UART port since only that port is available. How do I configure the UUU tool to flash the board using the UART port ?

0 Kudos
1 Solution
285 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

View solution in original post

0 Kudos
1 Reply
286 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @ahmedmd,

I hope you are doing well.

i.MX8QXP does not support flashing or downloading bootimage over UART.

It only supports USB 2.0 OTG and USB 3.0 ports.

Please refer to 5.10 Serial Downloader Boot in i.MX 8DualX/8DualXPlus/8QuadXPlus
Applications Processor Reference Manual for more information.

Thanks & Regards,
Dhruvit Vasavada

0 Kudos