Hi,
I am using imx8mq_evk to develop product and I execute UUU to flash images but it's can't finish.
The log is shown below
How can I fix this to complete flashing images?
UUU terminal
U:\sdk\fsl-imx-5.4.70\build-imx8mqevk-wayland-multilib\imx8_images\L5.4.70-2.3.0_images_MX8MQEVK> uuu -v -b sd_all imx-boot-imx8mqevk-sd.bin-flash_evk imx-image-full-imx8mqevk.wic
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.72-0-g8e9e189
Build in config:
Pctl Chip Vid Pid BcdVersion
==================================================
SDPS: MX8QXP 0x1fc9 0x012f [0x0002..0xffff]
SDPS: MX8QM 0x1fc9 0x0129 [0x0002..0xffff]
SDPS: MX8DXL 0x1fc9 0x0147
SDPS: MX28 0x15a2 0x004f
SDPS: MX815 0x1fc9 0x013e
SDPS: MX865 0x1fc9 0x0146
SDP: MX7D 0x15a2 0x0076
SDP: MX6Q 0x15a2 0x0054
SDP: MX6D 0x15a2 0x0061
SDP: MX6SL 0x15a2 0x0063
SDP: MX6SX 0x15a2 0x0071
SDP: MX6UL 0x15a2 0x007d
SDP: MX6ULL 0x15a2 0x0080
SDP: MX6SLL 0x1fc9 0x0128
SDP: MX7ULP 0x1fc9 0x0126
SDP: MXRT106X 0x1fc9 0x0135
SDP: MX8MM 0x1fc9 0x0134
SDP: MX8MQ 0x1fc9 0x012b
SDPU: SPL 0x0525 0xb4a4 [0x0000..0x04ff]
SDPV: SPL1 0x0525 0xb4a4 [0x0500..0x9998]
SDPU: SPL 0x0525 0xb4a4 [0x9999..0x9999]
SDPU: SPL 0x3016 0x1001 [0x0000..0x04ff]
SDPV: SPL1 0x3016 0x1001 [0x0500..0x9998]
FBK: 0x066f 0x9afe
FBK: 0x066f 0x9bff
FB: 0x0525 0xa4a5
FB: 0x18d1 0x0d02
FB: 0x3016 0x0001
Run built-in script:
uuu_version 1.2.39
# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f imx-boot-imx8mqevk-sd.bin-flash_evk
# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f imx-boot-imx8mqevk-sd.bin-flash_evk
# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f imx-boot-imx8mqevk-sd.bin-flash_evk -offset 0x57c00
SDPU: jump
# }
# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f imx-boot-imx8mqevk-sd.bin-flash_evk -skipspl
SDPV: jump
# }
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${sd_dev}
FB: ucmd mmc dev ${sd_dev}
FB: flash -raw2sparse all imx-image-full-imx8mqevk.wic
FB: flash bootloader imx-boot-imx8mqevk-sd.bin-flash_evk
FB: done
Wait for Known USB Device Appear...
New USB Device Attached at 1:41
1:41>Start Cmd:SDP: boot -f imx-boot-imx8mqevk-sd.bin-flash_evk
6400%1:41>Okay (0.585s)
New USB Device Attached at 1:41
1:41>Start Cmd:SDPV: delay 1000
1:41>Okay (1.004s)
1:41>Start Cmd:SDPV: write -f imx-boot-imx8mqevk-sd.bin-flash_evk -skipspl
99%1:41>Okay (4.644s)
1:41>Start Cmd:SDPV: jump
6400%1:41>Okay (0.325s)
And no more progress.
Target terminal
Boot SPL 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:27:39 +0000)
PMIC: PFUZE100 ID=0x10
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
Normal Boot
Trying to boot from USB SDP
SDP: initialize...
SDP: handle requests...
Downloading file of size 3030512 to 0x40400000... done
Jumping to header at 0x40400000
Header Tag is not an IMX image
Found header at 0x4040bfa0
U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e (Dec 04 2020 - 00:27:39 +0000)
CPU: i.MX8MQ rev2.1 1500 MHz (running at 1000 MHz)
CPU: Commercial temperature grade (0C to 95C) at 57C
Reset cause: POR
Model: NXP i.MX8MQ EVK
DRAM: 3 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C0 0x50]
MMC: FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... Run CMD11 1.8V switch
OK
[*]-Video Link 0imx8m_hdmi_probe
cdn_api_checkalive: keep-alive counter did not increment for 10us...
HDMI enable failed, ret -1!
(1280 x 720)
[0] display-controller@32e00000, video
[1] hdmi@32c00000, display
In: serial
Out: serial
Err: serial
BuildInfo:
- ATF f1d7187
- U-Boot 2020.04-5.4.70-2.3.0+ge42dee801e
Run CMD11 1.8V switch
switch to partitions #0, OK
mmc1 is current device
Detect USB boot. Will enter fastboot mode!
Net:
Warning: ethernet@30be0000 using MAC address from ROM
eth0: ethernet@30be0000
Fastboot: Normal
Boot from USB for mfgtools
*** Warning - Use default environment for mfgtools
, using default environment
Run bootcmd_mfg: run mfgtool_args;if iminfo ${initrd_addr}; then if test ${tee} = yes; then bootm ${tee_addr} ${initrd_addr} ${fdt_addr}; else booti ${loadaddr} ${initrd_addr} ${fdt_addr}; fi; else echo "Run fastboot ..."; fastboot 0; fi;
Hit any key to stop autoboot: 0
## Checking Image at 43800000 ...
Unknown image format!
Run fastboot ...
And no more progress.
Please guide me.
Thanks.
解決済! 解決策の投稿を見る。
This problem is cleared by retrying after disconnecting all cables with EVK board and power cycle my PC.
I guess USB Type-C connection was unstable.
This problem is cleared by retrying after disconnecting all cables with EVK board and power cycle my PC.
I guess USB Type-C connection was unstable.