Hi All,
I am trying to flash SPI flash memory in iMX8QX board with SCUFW along with the uboot. The iMX board has Linux v4.14.98, and I have built the SCUFW using imx-scow-porting-kit-1.3.0, uboot imx_v2018.03_4, UUU_1.3.0 and also the latest UUU. But whenever I try to use the command:
uuu -b qspi flash_uboot.bin flash.bin
I am getting the following error: "
nikola@NikolaTesla:iMX8QX$ sudo uuu -b qspi flash_uboot.bin flash_scfw.bin
uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.3.154-0-g47ddef5
Success 0 Failure 1
1:1 1/ 1 [HID(W):LIBUSB_ERROR_IO ] SDPS: boot -f flash_uboot.bin -skipfhdr
"
I have tried several different image even the prebuilt image "
sudo uuu -b qspi imx-boot-imx8qxpmek-fspi.bin-flash_flexspi
"
But both returns the same error. How to fix this issue?
Thanks and Regards
Ramprakash
How about use this "
sudo ./uuu -v -b qspi imx-boot-imx8qxpmek-fspi.bin-flash_spl_flexspi
"