USB host doesn't work at High Speed in i.MX25

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB host doesn't work at High Speed in i.MX25

ソリューションへジャンプ
1,202件の閲覧回数
fmvalero
Contributor II

Hi,

I'm working in custom board based on i.MX25 PDK. I have a USB 2.0 hub (USB2512B) attached to USBPHY2 (USB Host), and I don't get it to work at High Speed (the hub is detected as a Full Speed device). The USB OTG, however, is working at HS without problem. I was told that USBPHY2 is a serial PHY that can only work at Full Speed. Can anyone confirm that it is true? I haven't found official information about this.

Otherwise, what would I have to do to have it working at High Speed? Is there something in the kernel I have to modify? I have tried kernel 2.6.31 and 3.2.60, in both cases the result is the same (full speed).

Thanks,

Fernando.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
953件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fernando.

yes, i.MX25 has High speed USB Host with internal FS PHY,

if using internal PHY it is working only as Full Speed.

For High Speed one needs to use external ulpi phy transceiver

(from i.MX25 side this is signals : USBH2_STP, USBH2_NXT, USBH2_DATA[n]...).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
954件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Fernando.

yes, i.MX25 has High speed USB Host with internal FS PHY,

if using internal PHY it is working only as Full Speed.

For High Speed one needs to use external ulpi phy transceiver

(from i.MX25 side this is signals : USBH2_STP, USBH2_NXT, USBH2_DATA[n]...).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
953件の閲覧回数
fmvalero
Contributor II

OK. Thank you for your answer.

0 件の賞賛
返信