CPU: i.MX6 solo
BSP version: 3.10.17
Application: Car AVN
My customer wants to implement iOS Carplay solution for his product.
Could you help me to get USB dual role patch for USB driver in 3.10.17 BSP?
解決済! 解決策の投稿を見る。
Got a patch from SH AE team.
Hi,
Would it be possible for you to share the patch you received, or to put me in contact with the people you received the patch from?
Thanks
another problem: (Android 5.0)Patch code for i.MX6Q failed. c_patch does't work
We want to run android 5.0 on our I.MX6Q. We download the source code,freescale kernel,U-boot,path. Following the Android User's Guide, we now having a problem when patching. After running source /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga/and_patch.sh and enters help, it shows this:
Invoke ". and_patch.sh" from your shell to add following functions to your enviroment:
-- c_gotop: Change directory .....
-- c_patch: Recover working tree...
Then, running c_patch /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga imx_l5.0.0_1.0.0-ga does't work. It shows c-patch: commond not found. Why c_patch does't work? Was it really add c_patch function sucessfully when running “ source /opt/android_L5.0.0_1.0.0-ga_core_source/code/l5.0.0_1.0.0-ga/and_patch.sh”. How can we patch sucessfully?
Thank you
Hi Yong
dual-role mode (otg) is implemented in chipidea usb driver,
refer to Linux Manual sect.41.2.6 Changing the Controller Operation Mode,
controller mode is defined at dt file, eg arch/arm/boot/dts/imx6q-sabresd.dts
dr_mode = “otg” /* Set controller as otg mode */
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------