USB device not detected

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB device not detected

1,930件の閲覧回数
vincent_pelissi
Contributor I

Hello everyone,

I am designing a custom board with an i.MX6ULL processor with Linux version 4.14.78.

The uuu tool succeed in programming the eMMC with the fsl-image-qt5-validation-imx-imx6ull14x14evk.sdcard.bz2 file by using the USB port. When the board is ready (u-boot loaded and command prompt available on serial link), I plug a USB key but nothing appears (dmesg don't show any change). On previous prototype cards with same hardware the USB key was detected.

With memtool utility I have the following values on the registers PMU_REG_3P00 and PMU_MISC10:

root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8120 1
E
Reading 0x1 count starting at address 0x020C8120

0x020C8120: 00011775

root@imx6ull14x14evk:/# unit_tests/memtool -32 0x020C8160 1
E
Reading 0x1 count starting at address 0x020C8160

0x020C8160: 00030000

This values are the same on the working and not working boards. The voltage on VDD_USB_CAP pin is 3.2V as expected. The USB key is supplied with an external +5V regulator.

My question is why USB key is not detected whereas uuu has successfully programmed the eMMC over USB port?

Thank you for your help.

VP

0 件の賞賛
返信
1 返信

1,920件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi vincent_pelissi

 

for usb stick please check that USB_ID signal is low, for uuu tool

i.MX is working as usb device and this signal is high or floating.

 

Best regards
igor

0 件の賞賛
返信