Hello,
on iMX8Qm when I set the USB port to OTG mode (by setting the USB_OTG2_ID pad) the power enable pad (SS3_TC0) voltage drops, causing in a drop of the Vbus on the OTG port.
This is actually correct by reading the OTG specification. However, is it possible to control the SS3_TC0/USB_OTG1_PWR signal, regardless of the OTG/host status?
Thank you!
Francesco
解決済! 解決策の投稿を見る。
Hi Francesco
>Is it possible to keep the Vbus in OTG mode by reconfiguring some register?
not.
Best regards
igor
Hi Francesco
seems one can reconfigure SS3_TC0 as GPIO4_IO03 and make
necessary modifications in driver.
Best regards
igor
Hi Igor,
I know that muxing to GPIO is a possible solution. However, we cannot do that since in SCU FW port the GPIO4 device is assigned to a reserved HW partition.
Is it possible to keep the Vbus in OTG mode by reconfiguring some register?
Hi Francesco
>Is it possible to keep the Vbus in OTG mode by reconfiguring some register?
not.
Best regards
igor