Hello,
I am working on a custom imx6 solo board based on sabre-auto board. I am using linux-imx 3.10.17 version.
I am getting issue with USB_OTG. Whenever the board is set in gadget mode (g_serial module is loaded), I get the connection logs. But when i remove the serial cable from the board,
I dont get any disconnect logs. I tried monitoring for udev events using udevadm utility. Even udevadm does not give any disconnect events.
What can be done to enable/ detect the disconnect events.?
-Thanks
Sharvari Harisangam
Hi,
You could refer to the following threads:
About a USB driver of LinuxBSP for i.MX6 Solo
Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------