Hello together,
I want to drive a Dual-Channel LDSV Display with 1920 x 1200 from Sabre SD Board.
The Sabre SD Board offers me two different LVDS connectors, so I can do a Connection from the board to my Panel using even and odd signals.
How and where can I adjust in the Software (Android), so the i.MX6 generates Dual-Channel LVDS Signal so the odd Signal on LVDS0 and the even Signals on LVDS1?
Thank you very much for any Kind of Support.
Michael
Hi Michael
one can try to use kernel parameter ldb=spl0/1, refer to attached Release Notes
p.9, patch and link. Note lcd timings also should be adjusted
iMX6QD How to Add 24-bit LVDS Support in Android
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------