Troubles with OpenCL and iMX6Q Vivante

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Troubles with OpenCL and iMX6Q Vivante

1,033件の閲覧回数
ebn
Contributor I

Hi,

I'm trying to use OpenCL on a Sabrelite board based on iMx6 Q chip from element14. (soc reference : IMX6Q6AVT 10AC)

I have some weird troubles:

  • When I trace the max work items size i get this result:

Max work items dimensions: 3

Max work items size[0]:1024

Max work items size[1]:1024

Max work items size[2]:1024

Max work group size:1024

But when I try to run a kernel I got different limitations. For instance, with a very simply kernel just running this operation:

a[get_local_id(0)] = b[get_local_id(0)] + c[get_local_id(0];

I'm not able to run more than 128 work items / work group and the global work size is limited to 65536.

Why am I not able to run 1024 work items? Why I'm limited to 65536 for the global work size?


  • I'm trying to run a kernel that doing an image resample using OpenCL Image2D. To to this, my kernel is just calling the method read_image_f method for each pixels I want to write in the output buffer.

I encounter the same problem before but with no solution!

When my local work size is invalid, I reduce it and so I get the message that my global work size is invalid, so I reduce the global work size and I get the message that my local work size is invalid. For instance:

LWS = [8, 8, 0]  -> ok it's <= to 256

GWS = [256, 256, 0] -> ok it's <= 65536

------> INVALID GLOBAL WORK SIZE

LWS = [8, 8, 0]  -> ok it's <= to 256

GWS = [128, 128, 0] -> ok it's <= 65536

------> INVALID LOCAL WORK SIZE

LWS = [4, 4, 0]  -> ok it's <= to 256

GWS = [128, 128, 0] -> ok it's <= 65536

------> INVALID GLOBAL WORK SIZE

LWS = [1, 1, 0]  -> ok it's <= to 256

GWS = [1, 1, 0] -> ok it's <= 65536

------> INVALID GLOBAL WORK SIZE

So I don't understand how I can configure the execution dimensions to be compliant with the hardware.

For information, when I trace work group info for this last kernel, I got this informations:

Work group size : 48

Compile work group size 0 : 0

Compile work group size 2 : 0

Compile work group size 3 : 0

Local mem size : 0

Prefered work group size multiple : 16

Private mem size : 0

Thanks for any help!

Etienne

ラベル(2)
0 件の賞賛
返信
1 返信

529件の閲覧回数
shashankshivaku
Contributor I

Take a look at CL_KERNEL_WORK_GROUP_SIZE using clGetKernelWorkGroupInfo(). For Vivante GC2000, its 192. That is, for a particular kernel the max number of work items would be 192.

0 件の賞賛
返信