To use jffs2 file system by i.MX6 GPMI.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

To use jffs2 file system by i.MX6 GPMI.

跳至解决方案
1,325 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL GPMI.

Our partner want to use jffs2 file system, but Linux BSP (L3.0.35_4.1.0) cannot handle it by default, can it?

Then, we found the following URL.

[v4,06/12] mtd: gpmi: rewrite the gpmi_ecc_write_oob() to support the jffs2 - Patchwork

According to this URL, we can use jffs2 with the patch, but it seems that we have to input .ecobytes and .eccpos in gpmi_hw_ecclayout.

Then, could you let me know what value should we input to them?

Best Regards,

Satoshi Shimoda

标签 (5)
标记 (1)
0 项奖励
回复
1 解答
901 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Freescale currently does not support jffs2 for i.MX6 gpmi.

Actually driver currently is under development, not sure that it

is possible to provide now details.

Please post this question on mailing list link below, devoted to

development of NAND MTD drivers

http://lists.infradead.org/pipermail/linux-mtd/2013-October/049305.html

gpmi-nand driver and jffs2 support - Patchwork

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
902 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

Freescale currently does not support jffs2 for i.MX6 gpmi.

Actually driver currently is under development, not sure that it

is possible to provide now details.

Please post this question on mailing list link below, devoted to

development of NAND MTD drivers

http://lists.infradead.org/pipermail/linux-mtd/2013-October/049305.html

gpmi-nand driver and jffs2 support - Patchwork

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复