Could not recieve data on UART4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could not recieve data on UART4

2,038件の閲覧回数
koperapune
Contributor II

I am trying to configure UART4. I have added

MX6SL_PAD_KEY_ROW6__UART4_TXD

and

MX6SL_PAD_KEY_COL6__UART4_RXD

in mx6sl_brd_pads[ ].

Above pin configs are defined as

#define MX6SL_PAD_KEY_ROW6__UART4_TXD                                         \

        IOMUX_PAD(0x04AC, 0x01A4, 1, 0x0000, 0, MX6SL_UART_PAD_CTRL)

      

#define MX6SL_PAD_KEY_COL6__UART4_RXD                                         \

        IOMUX_PAD(0x048C, 0x0184, 1, 0x0814, 2, MX6SL_UART_PAD_CTRL)

I crosschecked these configs and looks like these configs are correct..

I have also called "imx6sl_add_imx_uart(3,NULL)" from function mx6_evk_init()

I configured UART5 just same as UART4. UART5 works well where as UART4 sends data correctly however could not receive it.

Would you please provide me pointers to solve this problem.


ラベル(1)
2 返答(返信)

1,799件の閲覧回数
boris-benshapir
Contributor II

Did you manage to solve? I'm having a similar issue... please help

0 件の賞賛
返信

1,799件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Please double check the daisy chain setting of the input pin UART4_RXD.

For your reference, some discussions about the UART pins.  https://community.freescale.com/message/340463#340463

Hope this can help you.