To use external clock with spread spectrum for i.MX6 IPU/LDB.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

To use external clock with spread spectrum for i.MX6 IPU/LDB.

Jump to solution
2,001 Views
satoshishimoda
Senior Contributor I

Hi community,

I want to confirm the specification of i.MX6 PLL in CCM module.

Actually, I want to use a external clock with spread spectrum via CLK1_N/CLK1_P pin to IPU, LDB as following route.

external clock -> CLK1_N, CLK1_P -> PLL5(CCM_ANALOG) -> CCM -> IPU, LDB

In this case, I think spread spectrum is preserve if I set PLL5 to bypass mode by BYPASS bit (CCM_ANALOG_PLL_VIDEOn[16] in chapter18.7.11 of IMX6DQRM Rev.1).

Is this correct?

Or spread spectrum will be cancelled by PLL5 even if it is set to bypass mode?

Best Regards,

Satoshi Shimoda

Labels (4)
Tags (2)
0 Kudos
Reply
1 Solution
1,242 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As per the RM the System PLL or PLL2 is the one that features spread spectrum.

And it is different to the video PLL or PLL5. Therefore the spread spectrum should be preserved in case you want to bypass the PLL5.

Best Regards,

Alejandro

View solution in original post

0 Kudos
Reply
1 Reply
1,243 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi,

As per the RM the System PLL or PLL2 is the one that features spread spectrum.

And it is different to the video PLL or PLL5. Therefore the spread spectrum should be preserved in case you want to bypass the PLL5.

Best Regards,

Alejandro

0 Kudos
Reply