Hello everyone:
We have a development board MCIMX6QP-SDB. And we need to program EMMC.
According to the instructions, we use L4.9.88 mfgtools. However, this version of mfgtools can not recognize board.
The following is running screenshots.
And report an error when we send electricity to the board.
The following is error screenshots.
The following is the log of mfgtools.
If we use l3.14.38.6ul verson of mfgtools, it could recognize board. But when the program EMMC into second step, our board can not be recognized.The following is the screenshots of l3.14.38 mfgtools in second step.
Our host environment is WIN7. The following is the screenshots of host environment.
So, could anyone can tell us how to program the EMMC?
And whether or not it is related to the setting of switch6?
Thanks.
Have you the i.MX6 HID driver properly installed on your host PC? Please check.
Also, please try the earlier MFGtools version, e.g. 4.9.11 or 4.1.15.
Also, what do you mean as the 'switch6'? Please specify.
Have a great day,
Artur