The power dissipation of i.MX 6DualLite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The power dissipation of i.MX 6DualLite

574件の閲覧回数
chris_zhang
Contributor II

Hi All.

We used the i.MX6 DualLife in the production, the Power dissipation of processors is large, the surface temperature is more than 70℃, now we wants to reduce the power dissipation:

1.Used the USB module, the data of USB write in DDR without ARM core.

2.The power of VPU and GPU are connectted together, we want to use the VPU without the GPU on.

3.We need to use the below processor inter module: USB, IPU, EMMC, MIP, DDR, and close the others.

Can you help to realize the request?

ラベル(1)
0 件の賞賛
返信
1 返信

516件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Chris

nxp has special service for such hardware and software optimizations, Professional Services

NXP Professional Services | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信