The RT1052 uses both QSPI FLash and QSPI PSRAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

The RT1052 uses both QSPI FLash and QSPI PSRAM

跳至解决方案
1,781 次查看
Maxwell_Liu
Contributor I

We want to use RT1052 to drive an 800*600 RGB interface display, but due to the lack of OCRAM space, we need external SDRAM, but the market of 16Bit SDRAM is seriously out of stock, we want to use SQPI PSRAM as video memory. The RT1052 FLXSPI supports port A and port B. I am wondering if QSPI Flash(W25Q64) can be mounted on port A and QSPI PSRAM(APS6404L) can be mounted on port B.

标签 (1)
0 项奖励
回复
1 解答
1,740 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) )If the above method works,can PSRAM be divided into two areas, one as program code area, the other as video memory and program running memory?
-- Yes, it's possible.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,734 次查看
Maxwell_Liu
Contributor I

Thank you very much

0 项奖励
回复
1,777 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) I am wondering if QSPI Flash(W25Q64) can be mounted on port A and QSPI PSRAM(APS6404L) can be mounted on port B.
-- Yes, you can, however, it's impossible for FlexSPI to access the QSPI and PSRAM simultaneously, in other words, the PSRAM can't replace the SDRAM in the RT1052's design.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,776 次查看
Maxwell_Liu
Contributor I

1)Is it possible to load all the APP code in QSPI FLAH into OCRAM during startup so that PSRAM can be used as video memory or even as program RAM

2)Is it possible to transfer all APP code in QSPI FLAH to PSRAM during startup, run code in XIP mode in PSRAM while PSRAM is used as video memory

0 项奖励
回复
1,753 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Is it possible to load all the APP code in QSPI FLAH into OCRAM during startup so that PSRAM can be used as video memory or even as program RAM
-- Yes, it's possible.
2) Is it possible to transfer all APP code in QSPI FLAH to PSRAM during startup, run code in XIP mode in PSRAM while PSRAM is used as video memory
-- No, I'm afraid not.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
1,746 次查看
Maxwell_Liu
Contributor I

I'm still a little confused about the second question.What is the problem with this solution not working, is it not able to automatically move APP code to PSRAM at startup, or is it not possible to use QSPI RAM as both XIP mode and video memory?

1)If I write a BOOT program, first start the BOOT program normally from QSPI Flash, and load the BOOT to ITCM to run, the function of BOOT is to copy all APP data in QSPI Flash to PSRAM. Can I then run the program directly on PSRAM in XIP mode.

2)If the above method works,can PSRAM be divided into two areas, one as program code area, the other as video memory and program running memory

0 项奖励
回复
1,741 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) )If the above method works,can PSRAM be divided into two areas, one as program code area, the other as video memory and program running memory?
-- Yes, it's possible.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复