The Android automotive 12 doesn't go to the deep sleep mode completely.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The Android automotive 12 doesn't go to the deep sleep mode completely.

2,995 Views
Ziegfried
Contributor I

Hello NXP team,

I use imx8qmmek board and automotive-12.0.0_1.1.0_image_8qmek_car2 build. When I run command "echo "1 2" > /sys/devices/platform/vehicle-dummy/power_req' to send the system to the "Suspend-to-RAM" mode the system doesn't go to the mode. It is seen by ftrace log(see ftrace.log).  In ftrace.log file I added two logs of Android 10 and Android12 for comparing.

 
 

I set power policy in the suspend mode(see pic.)

Also I see active wakelocks(see wakelocks.log).

How can I switch it off?

Thank you.

 

 

 

0 Kudos
Reply
9 Replies

2,976 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Do you connect the usb port when you use this command ?

0 Kudos
Reply

2,958 Views
Ziegfried
Contributor I

Yes, I do. I use just mini-usb connection. And I tried to send the system to sleep mode without usb-connection with script. A result is the same. Rootcouse is not in the usb connection.Please, help me.

 

T

0 Kudos
Reply

2,936 Views
martin_durak
NXP Employee
NXP Employee

Hi @Ziegfried 

 

could you try to suspend AA12 with the power button on the board? To go into suspend mode, you need to have disconnected USB, Ethernet...

 

Martin

0 Kudos
Reply

2,906 Views
Ziegfried
Contributor I
Power button doesn't go system to the sleep mode completely.
0 Kudos
Reply

2,903 Views
martin_durak
NXP Employee
NXP Employee

I suppose that until cca 7 s it goes to suspend mode, doesn`t it? Because after this time battery interrupt wake up system. It is build in function in kernel.

Another tip, is to make sure with ifconfig, that every connected module like (BT, ...) is disabled.

We also find out, that

echo "1 2 " > /sys/devices/platform/vehicle-dummy/power_req

doesn`t work, because if we use

echo $(</sys/devices/platform/vehicle-dummy/power_req)

the value is 1 0 and not 1 2...

 

BR

Martin

 

 

 

 
0 Kudos
Reply

2,889 Views
martin_durak
NXP Employee
NXP Employee

Hi @Ziegfried ,

 

for better undertanding could you share with us logs in this way.

logcat -b all -c

Enter to suspend mode

logcat -b all

and share with us this log.

 

Martin

0 Kudos
Reply

2,875 Views
Ziegfried
Contributor I

Hi, Martin.

I share log, how you requested.

There are the wakelocks in the power save mode:

mek_8q:/ $ dumpsys suspend_control_internal

-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
| WAKELOCK STATS |
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
| NAME | PID | TYPE | STATUS | ACTIVE COUNT | TOTAL TIME | MAX TIME | EVENT COUNT | WAKEUP COUNT | EXPIRE COUNT | PREVENT SUSPEND TIME | LAST CHANGE |
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
| PowerManagerService.Broadcasts | 699 | Native | Inactive | 1 | 161ms | 161ms | --- | --- | --- | --- | 549526ms |
| PowerManagerService.Display | 699 | Native | Inactive | 1 | 526641ms | 526641ms | --- | --- | --- | --- | 549365ms |
| PowerManager.SuspendLockout | 699 | Native | Inactive | 1 | 526619ms | 526619ms | --- | --- | --- | --- | 549346ms |
| ApmOutput | 505 | Native | Inactive | 274 | 208ms | 23ms | --- | --- | --- | --- | 549057ms |
| ApmAudio | 505 | Native | Inactive | 172 | 770ms | 103ms | --- | --- | --- | --- | 548745ms |
| PowerManagerService.WakeLocks | 699 | Native | Active | 4 | 1542374ms | 1541529ms | --- | --- | --- | --- | 1573116ms |
| usb_wakelock | 501 | Native | Active | 1 | 1543910ms | 1543910ms | --- | --- | --- | --- | 1573116ms |
| usb | --- | Kernel | Inactive | 1 | 0ms | 0ms | 1 | 0 | 0 | 0ms | 2500ms |
| inotify | --- | Kernel | Inactive | 5 | 154ms | 87ms | 5 | 0 | 0 | 0ms | 46112ms |
| alarmtimer.0.auto | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| [timerfd] | --- | Kernel | Inactive | 2 | 10ms | 6ms | 2 | 0 | 0 | 0ms | 27865ms |
| sc-powerkey | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| tcpm-source-psy-4-0051 | --- | Kernel | Inactive | 6 | 0ms | 0ms | 6 | 0 | 0 | 0ms | 4753ms |
| [timerfd] | --- | Kernel | Inactive | 35 | 29ms | 5ms | 35 | 0 | 0 | 0ms | 947856ms |
| [timerfd] | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| event1 | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| mmc0 | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| eventpoll | --- | Kernel | Inactive | 45 | 0ms | 0ms | 45 | 0 | 0 | 0ms | 947856ms |
| | --- | Kernel | Inactive | 114 | 145ms | 130ms | 114 | 0 | 0 | 0ms | 1552338ms |
| battery | --- | Kernel | Inactive | 1 | 0ms | 0ms | 1 | 0 | 0 | 0ms | 2493ms |
| eventpoll | --- | Kernel | Inactive | 119 | 0ms | 0ms | 119 | 0 | 0 | 0ms | 1552338ms |
| scu:rtc | --- | Kernel | Inactive | 1 | 0ms | 0ms | 1 | 0 | 0 | 0ms | 27858ms |
| [timerfd] | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| mmc1 | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| [timerfd] | --- | Kernel | Inactive | 8 | 14ms | 5ms | 8 | 0 | 0 | 0ms | 690409ms |
| event0 | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
| [timerfd] | --- | Kernel | Inactive | 0 | 0ms | 0ms | 0 | 0 | 0 | 0ms | 0ms |
-------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

Wakeups:


----- Suspend Stats -----
success: 0
fail: 0
failed_freeze: 0
failed_prepare: 0
failed_suspend: 0
failed_suspend_late: 0
failed_suspend_noirq: 0
failed_resume: 0
failed_resume_early: 0
failed_resume_noirq: 0

Last Failures:
last_failed_dev:
last_failed_errno: 0
last_failed_step:
----------


Suspend Info:
suspend attempts: 0
failed suspends: 0
short suspends: 0
total suspend time: 0 ms
short suspend time: 0 ms
suspend overhead: 0 ms
failed suspend overhead: 0 ms
new backoffs: 0
backoff continuations: 0
total sleep time between suspends: 0 ms

 

Thank you!

0 Kudos
Reply

2,836 Views
martin_durak
NXP Employee
NXP Employee

Hi @Ziegfried ,

it seems like you are not using NXP standard image, otherwise, it would go to suspend mode. From the log it can be seen, that your custom service, preventing to go into suspend mode.

Unfortunately, I can`t help you with such case. Maybe try to look at privileges or try to disable your custom service to see if it helps.

 

Martin

 

 

0 Kudos
Reply

2,907 Views
Ziegfried
Contributor I
I disconnected from USB, Ethernet. It didn't help.
0 Kudos
Reply