Testing signed images

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Testing signed images

跳至解决方案
740 次查看
eduardo3
Contributor III

Hello,

I am in the process of adding signed images to our board but I was left with questions on how to test that.

After getting a signed os_cntr_signed.bin image, it boots fine. On u-boot when I try ahab_status, I see SECO events (because I don't have my keys fused yet).

Initially I thought I could use u-boot fuse override for testing the fuse values I need to use, but that is not implemented. After searching on how to use fuse shadow registers, I found that it is not possible. Examples:

https://community.nxp.com/t5/i-MX-Processors/Access-to-OCOTP-registers-from-SCU-on-IMX8QM-leads-to-h...

https://community.nxp.com/t5/i-MX-Processors/IMX8-unable-to-override-OCOTP-shadow-registers-Is-there...

Initially If thought I could implement something like what is mentioned in the first link.

Based on that, how am I supposed to test secure boot keys / commands without permanently fusing the keys or bricking the board?

What is NXP advice on that?

For reference, we are using i.MX8X (imx8qxp).

 

0 项奖励
回复
1 解答
693 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If not burning the SRK fuse, you may can use OPENSSL command to analyze the images with their key.

 

Regards

在原帖中查看解决方案

0 项奖励
回复
2 回复数
664 次查看
eduardo3
Contributor III

I'll try the openssl approach in the future. Another FAE we contacted also confirmed there is no way of testing on a imx8 board without fusing the keys. His suggestion in that case was to fuse (if we are fine with that) but not close the device.

0 项奖励
回复
694 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

If not burning the SRK fuse, you may can use OPENSSL command to analyze the images with their key.

 

Regards

0 项奖励
回复