TVP5150 set routing information

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TVP5150 set routing information

820 Views
MicMoba
Contributor V

Hi,

how can I set the routing of the TVP5150 from userspace? Is there a way to do this over v4l2-ctl?

I saw in the kernel driver that there is an initalisation for an v4l2_i2c_subdev and there is a function selmux, but how can I control this function?

Thanks.

Labels (4)
Tags (3)
0 Kudos
Reply
1 Reply

735 Views
igorpadykov
NXP Employee
NXP Employee

Hi Michael

unfortunately nxp bsps do not support tvp5150, it is supported in compulab software

CM-FX6 Freescale i.MX6 SW Resources - Compulab Mediawiki 

GitHub - varigit/linux-imx: i.MX Linux Kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply