TC359749xbg worked with 4 mipi csi lanes

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TC359749xbg worked with 4 mipi csi lanes

2,287 Views
cjt0701
Contributor I

TC359749xbg enable 4 Lane MIPI Csi failed,but 2 lanes worked well based on imx8mq-evk with 720p60.

0 Kudos
Reply
9 Replies

2,117 Views
cjt0701
Contributor I

TC358749xbg

0 Kudos
Reply

2,117 Views
joanxie
NXP TechSupport
NXP TechSupport

maybe can refer to the link as below:

https://community.nxp.com/thread/498568 

0 Kudos
Reply

2,117 Views
cjt0701
Contributor I

Hi 

when i set 4 lanes,

the log is :

[ 42.567539] skip frame 0 

what is the reason?

0 Kudos
Reply

2,117 Views
sijiniu-b17591
NXP Employee
NXP Employee

joanxie

Customer enable the 4 lanes now, but it doesn't work normal.  See the log for it. And below is what customer's problem.

使用tc358749 进行HDMImipi 通过csi 输入到imx8mq , 遇到使用12 两个 lanes csi可以正常播放图像,切换到1234四个lanes的时候,图像就不能正常播放,imx8mqmipi csi有接受到数据,dma已经数据从rx fifo拷贝到frame buffer, 但是后续就有继续感觉好像停止,fb1fb2的完成中断并没有交替工作, 不知道是什么原因引起的.

4 lanes是因为tc358749这个芯片1080p输出必须用 4 lane,两条lane带宽不够,两条Lane只能支持到720p60.

Customer use yocto-imx8-4.14.78-1.0.0_ga .

I let customer try

assigned-clock-rates = <266000000>, <333000000>, <66000000>.  But it no help. Could you help to look it. Thanks.

0 Kudos
Reply

2,117 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to your log file:

[drm] phy_cfg_hdp() num_lanes: 4, mode:3840x2160p60, color depth: 8-bit, encoding: 1

it seems that you set lane to 4 already, what resolution do you need? 4k@60? for imx8m, the max clock should be

assigned-clock-rates = <266000000>, <333000000>, <66000000>.

0 Kudos
Reply

2,117 Views
sijiniu-b17591
NXP Employee
NXP Employee

joanxie

There's no "[drm] phy_cfg_hdp() num_lanes: 4, mode:3840x2160p60, color depth: 8-bit, encoding: 1" in the log file.  Could you check again?  This is customer used "1280,height=720".

0 Kudos
Reply

2,117 Views
joanxie
NXP TechSupport
NXP TechSupport

sorry, should be " mxc-mipi-csi2_yav 30a70000.mipi_csi1: lanes: 4, name: mxc-mipi-csi2.0"

0 Kudos
Reply

2,117 Views
sijiniu-b17591
NXP Employee
NXP Employee

joanxie

What's your meaning? Do you mean the dts wrong? Or others. Customer need use 4 lanes.

0 Kudos
Reply

2,117 Views
joanxie
NXP TechSupport
NXP TechSupport

no, I mean that you board set lane to 4 correctly, have you changed anything source code besides clock? I got information that imx8mq can support 4 lanes, and app team have already tested this on the bare board successfully, did you measure the clock signal when set to assigned-clock-rates = <266000000>, <333000000>, <66000000>. ? any different?

0 Kudos
Reply