Supported resolution for iMX6 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported resolution for iMX6 series

Jump to solution
818 Views
DonnyChiu
Contributor II

We are considering using iMX6 for one of our projects that needs to drive a 1280x800 LCD.

This product doesn't need a lot of CPU power, and it doesn't really need GPU.

But seems like some of the lower-end iMX6 (like the UUL, UL) CPU can only support up to 1388x768.

Can iMX6UUL or UL reconfigure to support 1280x800 LCD resolution?

Or what is the lowest-end iMX6 that can support 1280x800 LCD via LVDS/MIPI interface?

0 Kudos
1 Solution
594 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned restriction about " up to WXGA(1366x768) resolution at 60 Hz"
relates mainly to general performance issue. This means, that it is possible to increase
(i.MX6UL LCDIF) resolution  for low (frame) frequencies.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
595 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned restriction about " up to WXGA(1366x768) resolution at 60 Hz"
relates mainly to general performance issue. This means, that it is possible to increase
(i.MX6UL LCDIF) resolution  for low (frame) frequencies.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------