Supported resolution for iMX6 series

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Supported resolution for iMX6 series

跳至解决方案
1,527 次查看
DonnyChiu
Contributor II

We are considering using iMX6 for one of our projects that needs to drive a 1280x800 LCD.

This product doesn't need a lot of CPU power, and it doesn't really need GPU.

But seems like some of the lower-end iMX6 (like the UUL, UL) CPU can only support up to 1388x768.

Can iMX6UUL or UL reconfigure to support 1280x800 LCD resolution?

Or what is the lowest-end iMX6 that can support 1280x800 LCD via LVDS/MIPI interface?

0 项奖励
回复
1 解答
1,303 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned restriction about " up to WXGA(1366x768) resolution at 60 Hz"
relates mainly to general performance issue. This means, that it is possible to increase
(i.MX6UL LCDIF) resolution  for low (frame) frequencies.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,304 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  The mentioned restriction about " up to WXGA(1366x768) resolution at 60 Hz"
relates mainly to general performance issue. This means, that it is possible to increase
(i.MX6UL LCDIF) resolution  for low (frame) frequencies.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------