Hello,
Our product is based on i.MX with a M4 core which handles NFC requrests. When NFC card tags the antenna, the application code in M4 reads the request via NXPNFCRdLib. The question is that:
1. Is there any suggestion (exsting tool or SW) that can simulate the process? We don't want the hardware stuff which is not that convenient from automation perspective.
2. Do we have API document for NXPNFCRdLib so at least we can figure if we can make the simulation base on it or not?
Thanks a lot.
Justin
I checked PN7150 document, there is emulation mode. Can we use PN7150+customized SW application code to emulate a NFC card in the emulation mode?
FYI.
We have EVK for i.MX8MM and PN7150. And you can refer to AN11679 to run the demo on PN7150.