Hi mates!
As I'm quite noob with iMX28 eval. board, i'd like to ask you some questions, but first I'll try to explain what I'm trying to do. I've developed a java application which is running fine on a Raspberry Pi. Now I've been asked to migrate that application to this board.
What I've done:
What I'd like to do:
Thanks a lot.
Thank you for the suggestions.
The problem I think i have is that I don't understand the installation process of the different capabilities. I come from the Raspberry Pi environment where i just had to write "apt-get install XXXXX" to have that installed. Here I know it's different but I can't understand the process.
I think LTIB is the answer but honestly I don't know from where to start.
another good tutorial
Timesys Getting Started Guide for Freescale i.MX28 EVK | Timesys Embedded Linux
apt-get install works on ubuntu images, while ltib provides target image just for linux.
~igor
So if I need java package, for example, i should put it inside ltib/roots folder and use the md_mx28.sh script in order to put it in the SD Card?
Thanks.
Hi Alex
suggest to start with
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor. I think it's going to be really useful but I came across a silly problem. I don't know hot to transfer files between my host PC and the board.
Any help would be appreciated.
Hi Alex
one can look at AN3875 sect.5.3 TFTP Host Setup
http://cache.nxp.com/files/dsp/doc/app_note/AN3875.pdf
~igor
Hello,
Another suggestion. As soon as you have SHH running on target, you could use SCP in Linux host PC to transfer files. Also WinSCP from Windows OS.
Luis