Hello
I'm working with iot-gate-imx8plus from compulab which integrate i.MX8M-Plus CPU and I have difficulties to use a specific screen with resolution 800x480 over HDMI interface.
From the reference manual of the processor, I have read the following:
HDMI 2.0a Tx supporting one display
Resolutions of: 740x480p60, 720x480p60, 1280x720p60, 1920x1080p60, 1920x1080p120, 3840x2160p30
So the resolution I want is not listed. Is it possible to achieve such resolution ?
I started working on the topic by setting a custom edid file, playing with video= kernel parameter to force 800x480 resolution, but still not working. The best I succeed to do is to have HDMI connected and weston complaining because the the HDMI interface has no modes available
Thanks for feedbacks about this topic (I see it has been discussed many times but no clear answer is done).
Joel
已解决! 转到解答。
Hello,
Problem was HDMY PHY clock values available in linux-imx. See https://community.nxp.com/t5/i-MX-Processors/Specific-HDMI-screen-resolution-quot-hdmi-phy-quot-cloc....
Joel
Sorry no, the only information about the hdmi driver is on the Linux reference manual
https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf
Regards