OS: Ubuntu 18.04
Some ERR occurs while "bitbake fsl-image-qt5"
Informations as follows, anyone have ideas?
I would appreciate it!
=====================================================================================
ERROR: fsl-image-qt5-1.0-r0 do_rootfs: Error executing a python function in exec_python_func() autogenerated:
The stack trace of python calls that resulted in this exception/failure was:
File: 'exec_python_func() autogenerated', lineno: 2, function: <module>
0001:
*** 0002:license_create_manifest(d)
0003:
File: '/home/cui/linux/tool/yocto/fsl-release-bsp/sources/poky/meta/classes/license.bbclass', lineno: 48, function: license_create_manifest
0044: pkg_dic = {}
0045: for pkg in sorted(image_list_installed_packages(d)):
0046: pkg_info = os.path.join(d.getVar('PKGDATA_DIR', True),
0047: 'runtime-reverse', pkg)
*** 0048: pkg_name = os.path.basename(os.readlink(pkg_info))
0049:
0050: pkg_dic[pkg_name] = oe.packagedata.read_pkgdatafile(pkg_info)
0051: if not "LICENSE" in pkg_dic[pkg_name].keys():
0052: pkg_lic_name = "LICENSE_" + pkg_name
Exception: OSError: [Errno 2] No such file or directory: '/home/cui/linux/tool/yocto/fsl-release-bsp/build/tmp/sysroots/imx6ull14x14evk/pkgdata/runtime-reverse/No'
ERROR: fsl-image-qt5-1.0-r0 do_rootfs: Function failed: license_create_manifest
ERROR: Logfile of failure stored in: /home/cui/linux/tool/yocto/fsl-release-bsp/build/tmp/work/imx6ull14x14evk-poky-linux-gnueabi/fsl-image-qt5/1.0-r0/temp/log.do_rootfs.2743
ERROR: Task 9 (/home/cui/linux/tool/yocto/fsl-release-bsp/sources/meta-fsl-bsp-release/imx/meta-sdk/recipes-fsl/images/fsl-image-qt5.bb, do_rootfs) failed with exit code '1'
the errors after command bitbake fsl-image-qt5
can anyone can clear this
bitbake fsl-image-qt5
WARNING: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git, attempting MIRRORS if available
WARNING: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git, attempting MIRRORS if available
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1149"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/devyocto/var-fslc-yocto/sources/poky/scripts/native-intercept:/home/devyocto/var-fslc-yocto/build_x11/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/devyocto/var-fslc-yocto/sources/poky/scripts:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/usr/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/usr/sbin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/usr/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/sbin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/recipe-sysroot-native/bin:/home/devyocto/var-fslc-yocto/sources/poky/bitbake/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/hosttools"; export HOME="/home/devyocto"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://code.qt.io/qt/qtbase.git /home/devyocto/var-fslc-yocto/downloads//git2/code.qt.io.qt.qtbase.git --progress failed with exit code 128, no output
ERROR: qtbase-native-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtbase-native/5.15.2+gitAUTOINC+40143c189b-r0/temp/log.do_fetch.2452
ERROR: Task (/home/devyocto/var-fslc-yocto/sources/meta-qt5/recipes-qt/qt5/qtbase-native_git.bb:do_fetch) failed with exit code '1'
ERROR: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure: Fetch command export PSEUDO_DISABLED=1; export DBUS_SESSION_BUS_ADDRESS="unix:path=/run/user/1000/bus"; export SSH_AGENT_PID="1149"; export SSH_AUTH_SOCK="/run/user/1000/keyring/ssh"; export PATH="/home/devyocto/var-fslc-yocto/sources/poky/scripts/native-intercept:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/usr/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/sysroots-uninative/x86_64-linux/usr/bin:/home/devyocto/var-fslc-yocto/sources/poky/scripts:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/usr/bin/x86_64-linux:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/usr/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/usr/sbin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/usr/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/sbin:/home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/recipe-sysroot-native/bin:/home/devyocto/var-fslc-yocto/sources/poky/bitbake/bin:/home/devyocto/var-fslc-yocto/build_x11/tmp/hosttools"; export HOME="/home/devyocto"; LANG=C git -c core.fsyncobjectfiles=0 clone --bare --mirror git://code.qt.io/qt/qtdeclarative.git /home/devyocto/var-fslc-yocto/downloads//git2/code.qt.io.qt.qtdeclarative.git --progress failed with exit code 128, no output
ERROR: qtdeclarative-native-5.15.2+gitAUTOINC+104eae5b17-r0 do_fetch: Fetcher failure for URL: 'git://code.qt.io/qt/qtdeclarative.git;name=qtdeclarative;branch=5.15.2;protocol=git'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/devyocto/var-fslc-yocto/build_x11/tmp/work/x86_64-linux/qtdeclarative-native/5.15.2+gitAUTOINC+104eae5b17-r0/temp/log.do_fetch.52577
ERROR: Task (virtual:native:/home/devyocto/var-fslc-yocto/sources/meta-qt5/recipes-qt/qt5/qtdeclarative_git.bb:do_fetch) failed with exit code '1'
WARNING: qtbase-5.15.2+gitAUTOINC+40143c189b-r0 do_fetch: Failed to fetch URL git://code.qt.io/qt/qtbase.git;name=qtbase;branch=5.15.2;protocol=git, attempting MIRRORS if available
Sorry, what do you mean about BSP, If is Board Support Package? I'm new one in this field.
I just want to build the rootfs for Qt development. It's known that Ubuntu 16 is recommended to build the yocto project, but all of my other work is based on Ubuntu 18.04, so I have to make a try.
Thanks for your reply.
Thanks,
BSP version: "NXP's 4.1.15-2.1.0 Yocto Project BSP" found in README-IMXBSP. Is it helpful?
Commands:
1. DISTRO=fsl-imx-x11 MACHINE=imx6ull14x14evk source fsl-setup-release.sh -b build
2. bitbake fsl-image-qt5