Hi,
If the SD3 interface is not used, is it okay to leave NVCC_HIGH and NVCC_LOW unpowered?
The only note I can find about leaving these unpowered is note 7 on page 26 of IMX6SXIEC data sheet that states:
"All digital I/O supplies (NVCC_xxxx) must be powered under normal conditions whether the associated I/O pins are in use or not and associated IO pins need to have a Pullup or Pulldown resistor applied to limit any floating gate current."
But this note doesn't reference NVCC_HIGH and NVCC_LOW.
Thanks,
Scott
已解决! 转到解答。
Hi Scott
expression "All digital I/O supplies (NVCC_xxxx) must be powered.."
relates to all power supplies beginning with NVCC_, so NVCC_HIGH and NVCC_LOW
should be powered too.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------