Dear Yuri,
Yes I understand the impact of the single channel to dual channel. However, what if I under some special condition and have to do that (single channel)? The special condition may mean a downgrade memory chip was mounted to board and it happens to have one bit data bus stuck at zero. So back to my original question, can I use single channel LPDDR4? If I use Linux to boot up, do I need to rebuild the kernel or just change some configurations in uboot?
Kayi
Hello,
Since LPDDR4 device consists of two identical channels operating independently, it is possible to
configure single channel x16 mode. But we do not have tested example for it. Customers can try
As for Linux - refer to chapter "Porting U-Boot" in "i.MX_BSP_Porting_Guide.pdf" in NXP Linux doc
package.
Regards,
Yuri.
Hello,
LPDDR4 is essentially dual channeled; using single channel means
half of memory is lost.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------