Shared ZQ resistor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shared ZQ resistor

Jump to solution
1,362 Views
george
Senior Contributor II

Dear OliverChen

How should we set Shared ZQ resistance in RPA when using LPDDR4 configured as shown below?

pastedImage_1.png

We do not share anything except Reset_n and RZQ in our schematics.

In such a case, should Shared ZQ resistor be DISABLED?

Best Regards,

George

Labels (1)
0 Kudos
1 Solution
1,192 Views
oliver_chen
NXP Employee
NXP Employee

Hi george‌,

I'm sorry the term of 'rank' confuses you. RANK used on DDR is chip select (CS).

"Shared ZQ resistor" can be either enabled or disabled in your configuration because there is only 1-rank (1-CS), but DISABLED is better.

B.R

Oliver

View solution in original post

4 Replies
1,192 Views
oliver_chen
NXP Employee
NXP Employee

Hi george‌,

How many RANKs do you use? If you only use one-rank LPDDR4, you can set "Enalbe/DIsable Shared ZQ resistor" to DISABLED. If you use two-rank LPDDR4 but you have two ZQ resistors, you also set it to DIABLED. Otherwise, you should set it to ENABLED

B.R

Oliver

1,192 Views
george
Senior Contributor II

Hi OliverChen

Please tell me one last thing.

I may not yet correctly understand the RANK you say.

We use i.MX8M.

Should the "Shared ZQ resistor" be set to Enable when using the LPDDR4 shown in the figure above with the configuration in the table below?

pastedImage_1.png

Best Regards,

George

0 Kudos
1,193 Views
oliver_chen
NXP Employee
NXP Employee

Hi george‌,

I'm sorry the term of 'rank' confuses you. RANK used on DDR is chip select (CS).

"Shared ZQ resistor" can be either enabled or disabled in your configuration because there is only 1-rank (1-CS), but DISABLED is better.

B.R

Oliver

1,192 Views
george
Senior Contributor II

Dear OliverChen‌,

Thanks.

0 Kudos