Send and receive CAN frames on i.mix 6 sabre auto(i.MX6xAI CPU2)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Send and receive CAN frames on i.mix 6 sabre auto(i.MX6xAI CPU2)

625 Views
manhtoan
Contributor II

Hello,

My first question Send and receive CAN frames on i.MX6xAI CPU2

I followed  MX_6DualQuad_6DualLite_SABRE_Auto_CPU2_Yocto_Project_Patch_Release_Notes.pdf

i met some problem but i try build more and it built done but when i push image on sdcard and run board, run  example in  SocketCAN - Wikipedia, the free encyclopedia

and i can't see any signal output. Could you help me? or show me version of Linux Binary Demo Files for me can run SocketCan on board.

Any help would be greatly appreciated.

0 Kudos
1 Reply

314 Views
igorpadykov
NXP Employee
NXP Employee

Hi manh

i.MX6 BSP supports only generic CAN APIs and  unfortunately SocketCan

is not supported. One can apply to mss or nxp software partners for developing

full ready solution.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos