AnsweredAssumed Answered

Send and receive CAN frames on i.MX6xAI CPU2

Question asked by manh toan on May 4, 2016
Latest reply on May 6, 2016 by igorpadykov

Hello,

i am new IMIX 6, currently i am using L3.10.53_1.1.0_iMX6QDLS_Bundle

for my board and it run.

but when i used example in  SocketCAN - Wikipedia, the free encyclopedia

to send data out using Can socket,

 

i config :

#ip link set can0 up type can bitrate 125000

root@imx6qdlsolo:/run/media/mmcblk2p1# ./demo_can_1

can0 at index 4

Wrote 16 bytes

 

i use oscilloscope to measure result sinal out but i can't see any thing.

First. i don't know can0 is J34 or J35 on my board  so i measure both, can0 is j34 or J35 ?

Second Please tell me why i can send can frame out (because of linux binary or some thing) help me

 

Any help would be greatly appreciated.

Outcomes