Hi,
Nothing is seen on seiko display (touch), when trying to boot IMX53-Ubuntu on start-R board. Can anybody help me in displaying GUI on touch. I'm able to display the GUI through VGA.
Thanks
Swaraj
解決済! 解決策の投稿を見る。
For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.
Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.
For the Seiko display, please try to add the "video=mxcdi0fb:RGB24,SEIKO-WVGA di0_primary" in the bootargs in u-boot.
Basically, you can check the BSP release note for all the bootargs parameters for kernel boot.
Hi Chin Fung Chan,
Thanks a lot. It worked for me. Now i have an other issue. Currently i'm using Ubuntu on IMX53, how should i enable virtual keyboard at login and for typing.
I think you talk about the on-screen keyboard. I didn't try it on the i.MX board. but I think the following information may useful for you.
1. http://cmwelsh.com/enable-on-screen-keyboard-ubuntu-lucid-lynx
Hi Randy,
I have IMX53 Start-R board with the following information on the board: SCH -27104 Rev B 700-27104 Rev X5. The link you have specified talks about the IMX53 QSB board.
Do we really need to do any modification on this version of Start-R boards to get the display. Please let us know.
Thanks,
Swaraj,
What are your uboot args?
Regards,
Randy Krakora
Field Applications Engineer
Freescale Semiconductor
(765)-860-6622