I'm using i.mx283 (i.MX283 Processors|High-Performance|NXP )
Couldn't find any documents on how to disable/partially disable JTAG port.
https://www.nxp.com/docs/en/application-note/AN4686.pdf Is this application note valid for i.mx28?
Is it possible to disable JTAG memory access(keeping boundary scan enabled) ?
Is it possible to do this without any manufacturing tools, directly from the Linux running on the processor?
Thanks,
- Abhijith
Hi Igor,
Thank you for the answer.
Could you explain, how can I burn the fuse bit from Linux?
-Abhijith
Hi Abhijith
yes this is possible burning bit0 fuse on address HW_OCOTP_CUSTCAP described in
sect. 20.4.18 Customer Capability Shadow Register (HW_OCOTP_CUSTCAP) i.MX28 Reference Manual
https://www.nxp.com/docs/en/reference-manual/MCIMX28RM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------