Seco version 3.7.1 throws unknown SECO Event[1] = 0x00DAF429

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Seco version 3.7.1 throws unknown SECO Event[1] = 0x00DAF429

ソリューションへジャンプ
219件の閲覧回数
Chandni
Contributor I

Hi Team,

I am wanting to use seco version 3.7.1 for my imx8 chip. However I get below seco events:
SECO Event[0] = 0x0087EE00
SECO Event[1] = 0x00DAF429

0x0087EE00 --> is not a problem as i did not OEM close my board and I am not using a signed image.

However, the other event  I am not sure what is wrong.
For 0x00DAF429:
Status byte: 0x29  is AHAB_FAILURE_IND
Ind byte: 0xF4 is AHAB_INVALID_MESSAGE_IND
0x00DA is not known, i assume it is a command, but its not documented anywhere.

2  questions:

  1. Could you please point me to a direction which could help me fix 0x00DAF429 error? As per your documents my board cannot go to OEM close with this seco event, correct?
  2. Can I downgrade seco firmware version say for example from 3.8.6 to 3.7.1?

Thanks in advance.

@Harvey021 

 

 

ラベル(1)
0 件の賞賛
返信
1 解決策
184件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Did reply back to meng hao who should also inform you the same.

 

Regards

Harvey

元の投稿で解決策を見る

1 返信
185件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hi,

Did reply back to meng hao who should also inform you the same.

 

Regards

Harvey