Saving Vcc power with i.MX537

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Saving Vcc power with i.MX537

跳至解决方案
1,037 次查看
TedMichon
Contributor I

I understand the DVFS concept with Vdd, but how does it work with Vcc? With Vdd, we just slow the CPU clock, and therefore can lower the voltage and save power while we aat idle or in background.

But with Vcc, we cannot lower the FEC or USB or UART clocks without causing the these systems to fail because they need specific clock rates. How does one save power with DVFS for Vcc?

-Ted

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
900 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Ted

     The DVFS includes CORE and PER, the CORE means CPU, and PER means peripheral, once there is no high speed devices running, dvfs per driver can lower bus's freq, includes DDR, AXI, AHB etc., and with lower bus freq, Vcc can be lower as well.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
900 次查看
YixingKong
Senior Contributor IV

Ted

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 项奖励
回复
900 次查看
YixingKong
Senior Contributor IV

Ted

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 项奖励
回复
901 次查看
AnsonHuang
NXP Employee
NXP Employee

Hi, Ted

     The DVFS includes CORE and PER, the CORE means CPU, and PER means peripheral, once there is no high speed devices running, dvfs per driver can lower bus's freq, includes DDR, AXI, AHB etc., and with lower bus freq, Vcc can be lower as well.

0 项奖励
回复