Hi all,
In my application, i need to switch the SPI1_SCLK and SPI1_MISO pin from SPI1 function to GPIO function on run time.
Below is how i do it in my driver:
#define MUX_CTL_MASK 0x07
#define _reg_SPI1_MISO_MUX_CTL (*(VUINT32 *)IO_ADDRESS(MX6Q_IOMUXC_BASE_ADDR + 0x7C))
#define SPI1_MISO_MUX_GPIO 0x05
#define SPI1_MISO_MUX_SPI 0x02
#define _reg_SPI1_SCLK_MUX_CTL (*(VUINT32 *)IO_ADDRESS(MX6Q_IOMUXC_BASE_ADDR + 0x74))
#define SPI1_SCLK_MUX_GPIO 0x05
#define SPI1_SCLK_MUX_SPI 0x02
void spi_pola_active_low()
{
//set clock/data to gpio
_reg_SPI1_MISO_MUX_CTL = (_reg_SPI1_MISO_MUX_CTL & ~MUX_CTL_MASK) | SPI1_MISO_MUX_GPIO;
_reg_SPI1_SCLK_MUX_CTL = (_reg_SPI1_SCLK_MUX_CTL & ~MUX_CTL_MASK) | SPI1_SCLK_MUX_GPIO;
return;
}
This implementation work successfully in i.MX6 SOLO board. However, in i.MX6 DUAL board, it fail. I am not able to toggle the SPI1_SCLK pin using normal GPIO setting. Kernel coding is the same for SOLO and DUAL board.
Is there any problem with my implementation? Appreciate some help here.
Thank you
Regards,
ZC
已解决! 转到解答。
Hi ZC
IOMUX are different for i.MX6DQ and SoloDuaLite, please recheck Chapter 36,37
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ZC
IOMUX are different for i.MX6DQ and SoloDuaLite, please recheck Chapter 36,37
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6DQRM.pdf
http://cache.freescale.com/files/32bit/doc/ref_manual/IMX6SDLRM.pdf
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------