SGTL5000 MIC. recording problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGTL5000 MIC. recording problem

1,512件の閲覧回数
ispark
Contributor I

Hi,

I uses SGTL5000 with i.mx6SL using Android 4.4.2.

Above audio codec can play wav file without problem.

While recording MIC input to wav file, audio broken sometimes.

for example, just record about 10 seconds but just plays about 8 seconds. that means some region plays shortly than expected time,  2 second voice just omitted(compressed).

we just no connected VDDD. 

Please let us know where should I check.

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,099件の閲覧回数
ispark
Contributor I

Additionally I have below results.

1. record by tinycap to wav file, then recorded sound file sometimes broken,

2. record by Android Sound Recorder using codec AMR(Adaptive Multi Rate), file does not have noise.

so it can record succesfully.

Does anybody have any idea why tinycap's recorded wav file are broken?

Thanks

IS

0 件の賞賛
返信

1,099件の閲覧回数
art
NXP Employee
NXP Employee

The most likely cause of the issue is a high amount of software overhead, produced by non-native software to the system. So, it's always better to use native applications.

Best Regards,

Artur

0 件の賞賛
返信

1,099件の閲覧回数
varunjeevangoud
Contributor I

Hi,

Imx6 Solo:  imx-sgtl5000 driver.

Mic recording comes only for 10 secs. When I playback (using android application), audio comes for only first 10 secs and after that no audio till the end of the recording. But the player continues till the end of recording.

There can't be a problem on the application.  Is there any limitation in sgtl5000 driver??

Pls. advise.

0 件の賞賛
返信